This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
在 空载情况下有5V输出,带上负载就没有输出,会不会是什么原因造成的
亲;如果你我换个位置,你能知道我在做啥吗?上图上波形和描述清你接的啥负载。
麻烦告知你二极管和电感的型号
加多大负载
二极管使用的是BR210,电感使用的是100uH的2A带屏蔽电感,负载只要带一点点就不行
加一点点就不行,
BR210,不行电感使用的是101的2A带屏蔽的电感