按照TLC5940推荐设计进行电路设计,外界单片机版进行驱动调试。
单颗TLC5940可以正常工作,16个通道均工作正常,但SOUT输出和SIN输入不匹配,如SIN输入16个0xFF,SOUT输出为3个0x00+13个0xFF,导致级联使用时有部分通道无法正常工作。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
按照TLC5940推荐设计进行电路设计,外界单片机版进行驱动调试。
单颗TLC5940可以正常工作,16个通道均工作正常,但SOUT输出和SIN输入不匹配,如SIN输入16个0xFF,SOUT输出为3个0x00+13个0xFF,导致级联使用时有部分通道无法正常工作。
在灰度数据输入模式(VPRG设置为GND)下,TLC5940的输入移位寄存器的宽度为192位,这意味着在第192 SCLK的下降边缘,第一个输入192位数据将在Sout上开始输出。 请注意,TLC5940的灰度PWM分辨率为12位。
例如,如果要将第一个TLC5940的所有PWM输出设置为50%(对应的灰度值为0x800),将第二个TLC5940设置为100%(对应的灰度值为0xFFF),则应发送16*0xFFF +16*0x800,如下所示。