This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM3478: DC 22V输入,如何降低启动电流在1A以内?

Part Number: LM3478

前段时间调好的LM3478反激两路输出,是用台式直流源直接供电的,带载正常,带载启动和突投载突卸载都正常。

测试了LM3478的启动,源端至少提供1.5A的电流(22V)才能启动。

但现在的实际应用是无台式直流源,前端直流源22V /1.2A,最大功率26.4W,无法提供更大电流。

LM3478工作频率为120KHz,CS采样电阻20mR,补偿端68nF和10K电阻

请问下,如何减小LM3478的启动功率,在源端提供22V/1A时,也能正常启动?