This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ25611D: BQ25611D设置20h长时间充电保护,24h后无法触发寄存器置位。

Part Number: BQ25611D


BQ25611D已经设置了20h的长时间充电保护,电池使用假电池代替,设定电池电压3.7V。充电24小时,无法触发寄存器置位。正常应该故障寄存器的 CHRG_FAULT 位(REG09[5:4])会被设置为 11。
但是读到寄存器没有被置位,同时没有自动停充,电池仍有200mA充电电流。VSYS仅对LED供电,电流14mA,VBAT电池脚仅对系统主芯片供电,电流20mA。