This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于bq24170不充电的问题

Other Parts Discussed in Thread: BQ24170

上电后,状态指示灯一阵闪烁,然后就常亮。检测一下充电的条件,都是符合的;

而且在状态灯常亮后,拔掉电池在插上,指示灯一直闪烁。拔掉电池,检测了一下sw的输出,一直是1V左右的电压。

望大神予以解答,万分感谢。

  • 亲;你的电路是咋连的?接的啥负载?

  • 通常客户调试时容易忽略NTC电阻,如果在你的调试电路中没有使用NTC器件但是偏置电路还是按照datasheet给定的偏置,那么会让IC误认为是出现低温,所以请检查一下NTC的位置是否有接,如果没有接调试时用个10K欧姆或100欧姆电阻替代之(取决于所选用NTC 25度室温下的电阻值)。以上谢谢!

  • 已经接上了,ts引脚的电压为2v左右,大概是20度。

    这个电压应该没问题吧

  • 基本没接负载,问题是不充电,电池是可以正常供电的

  • 已经接上了,ts引脚的电压为2v左右,大概是20度。

    这个电压应该没问题吧

  • 没有电池时,芯片会进行电池插入检测,输出端应该是一个周期性的脉冲电压(参考datasheet page 21)。

    建议楼主检查一下硬件连接,检查一下输出端电容是否正常。

    实验用的芯片建议从TI官网申请样片。 

    http://www.ti.com.cn/product/cn/BQ24170/samplebuy

  • 我是按照你们TI的EVM板的电路图画的,PCB也是仿照你们的,只是把充电电流改为500mA(经测量Viset为160mV),现在SW端的电感为8uH,电容为5.1uF,频率在24K。

    你看是不是因为电流太小了?

  • 测了一下电池的电流为6.6mA,这时候状态指示灯常亮,也就是state为OFF状态。

    芯片是申请样片的。芯片能输出3.3V,REGN端也是输出6V,但SW始终没有输出检测波形,我能认为芯片是坏的吗?

  • 充电电流设置小一点这个芯片也是可以支持的,楼主描述的现在电容为5.1uF 是指的哪一个电容?

    即具体在电路图上的电容编号是哪一个?谢谢!

  • 在实际焊接的时候,把C14,C15拿掉了,换成一个5.1uF的电容

  • 24KHZ是LC的双重极点的位置,因为兼容陶瓷类型的输出电容,所以采用了3型补偿器,内部补偿网络零点位置限制了LC极点位置在15-25KHZ之间。

    楼主 是否还有其他元器件的更换,或者任何与给定电路图上不一致的焊接。是否有换一个IC去验证一下。谢谢!

  • The following conditions have to be valid before charging is enabled:
    • ISET pin above 120 mV.
    • Device is not in UVLO mode (that is, V
    AVCC
    > V
    UVLO
    ).
    • Device is not in SLEEP mode (that is, V
    AVCC
    > V
    SRN
    ).
    • OVPSET voltage is from 0.5 V to 1.6 V to qualify the adapter.
    • 1.5-s delay is complete after initial power up.
    • REGN LDO and VREF LDO voltages are at correct levels.
    • Thermal Shutdown (TSHUT) is not valid.
    • TS fault is not detected.
    • ACFET turns on (see System Power Selector for details).
    One of the following conditions stops ongoing charging:
    • ISET pin voltage is below 40 mV.
    • Device is in UVLO mode.
    • Adapter is removed, causing the device to enter SLEEP mode.
    • OVPSET voltage indicates the adapter is not valid.
    • REGN or VREF LDO voltage is overloaded.
    • TSHUT temperature threshold is reached.
    • TS voltage goes out of range, indicating the battery temperature is too hot or too cold.
    • ACFET turns off.

    逐条对照,问题绝大部分是以上其一。