Other Parts Discussed in Thread: BQSTUDIO, EV2400, , BQ25756, BQ25750
在输入电压开始为11V时,其充电电压为EVM板子默认充电电压22V,在输入电压从11V增加到20V时,其充电电压从22V增加到接近30V.但输入电压达到21V时,其充电电压变为7V左右。设置输入电压大于20V时,其充电电压都小于默认充电电压。使用EV2400在BQStudio上查看芯片寄存器数据都在正常范围,请问这是板子哪方面出来问题了。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
在输入电压开始为11V时,其充电电压为EVM板子默认充电电压22V,在输入电压从11V增加到20V时,其充电电压从22V增加到接近30V.但输入电压达到21V时,其充电电压变为7V左右。设置输入电压大于20V时,其充电电压都小于默认充电电压。使用EV2400在BQStudio上查看芯片寄存器数据都在正常范围,请问这是板子哪方面出来问题了。
这种行为很奇怪,我以前从未见过。
BQ25756经过优化,可以在输出端连接电池或某种负载。如果你连接了电池或CV负载,这种行为会继续吗?
如果您连接了CV负载,请确保有一个1000µF或更大的电容器与CV负载并联。这将有助于CV负载更好地模拟电池。
此外,设置位EN_PFM=0、EN_PRECHRG=0或EN_TERM=0是否会改变这种行为?
我照着您这样设置设置位EN_PFM=0、EN_PRECHRG=0或EN_TERM=0,充电工况如下:
输入电压从11V输入,电池端20.393 V,没有输出电流,从11V逐渐增加到13V,恒压23.5V,没有输出电流。电压增加到15V,开始有电流0.0125A,电压增加到19V,电流增加到1.82A,电压增加到19.7V,电流2.18A,充电功率51.37W.输入超过20V时,降压电路工作,充电电压又变为8V。
当你说电流为2.18A或0.0125A时,你是指流入BQ25750的电流还是流出BQ25750?
VSYS上有负载吗?
这很奇怪,我认为这个EVM可能会损坏。只是为了澄清一下,在VSYS或VBAT上没有负载的情况下,EVM有2.18A?2.18A可能通过开关MOSFET或其他方式分流到GND。
你能检查开关FET是否损坏吗?
您是否尝试过使用不同的BQ25750EVM?