This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

bq24195带不动负载,接负载时输出电压降低



我的bq24195接负载有问题,当输出300mA时输出电压PMID从5.10降到4.8V,接600mA负载时PMID降到4.6V,换了1uH的电感,还是没什么大的变化,请问这是什么原因?是外部电路的问题吗?我的电感值是1uH,Cpmid使用的是3个22uF的陶瓷电容和1个0.1uF的陶瓷电容。软件应该不影响输出特性吧,需要的话,我把寄存器值贴出来