This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS7A47: 正负30V输入产生正5V、正3.3V、正3V以及负5V电压

Part Number: TPS7A47
Other Parts Discussed in Thread: LM337

您好,我想请教个问题。

在电路设计过程中,我的输入电压为正负30V,现在需要产生正5V电压、正3.3V电压以及正3V电压给ADC、DAC、晶振以及运放供电,然后需要产生-5V给运放供电。

我可以使用三个TPS7A4700将30V输入分别转换成正5V、正3.3V和正3V吗?可以使用TPS7A3001将负20V输入转换为负5V输出吗?

手册上似乎是满足的,但是输入输出的压差是否过大,存不存在问题?

或者使用LM337将负30V转换为负5V合适吗?

再或者进行过渡一下,将正负30V转换为正负10V,然后再转成需要的电压?