This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMR14206XMK/NOPB 输入18冒烟

Other Parts Discussed in Thread: LM2842, TPS62175, LMR14206

怎么用贵公司的LMR14206XMK/NOPB做5V输出的电源,我试着把输入电压从7V慢慢调整到18V,5V都可以正常输出,但是我把输入断开 直接把输入电压调整到18v IC直接冒烟。我试过贵公司的好几款高输入电源IC都是这样的情况,输入电压慢慢加大到18V不会出问题,如果直接18V输入就会烧。我仔细检查了电路没有发现问题。IC有从一级代理那里拿,换了有3,4家 情况都一样。

  • 我也有试过TPS62175和lm2842这两个IC,一样的问题, 输入18V左右就烧  ,没有带任何负载 ,输入是用可调电源。我现在需要输入电压范围是7到18V的IC,我选择的这3款IC 输入电压都远高于18V 搞不清楚,为什么都会烧 。在此向大家请教!谢谢!

  • LMR14206耐压超过40V,正常18V输入应该没有问题,很多客户这颗IC都是用在24V输入的。

    可以抓拍一下输入电压接上去一瞬间的电压、电流波形,看看有没有异常现象。

  • 同意Jeff Qiu的判断,建议抓下芯片VIN pin脚在18V电压加上瞬间的波形,你会看到一个极高的尖峰电压,远超过18V。这是一种热插拔过程,导线和输入电容二阶谐振,导致输入电压的尖刺。