我板子上有器件需要+-2.5V的电源,现在能提供的输入有+-5V电源,麻烦给推荐下电源管理芯片。另外电流需要200mA以上的,因为那个器件的工作电流能达到200mA,谢谢。期待尽早答复。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
我板子上有器件需要+-2.5V的电源,现在能提供的输入有+-5V电源,麻烦给推荐下电源管理芯片。另外电流需要200mA以上的,因为那个器件的工作电流能达到200mA,谢谢。期待尽早答复。
推荐选用LDO产生-2.5V, 如TPS72325, TPS72301等等。 2.5V可选用TLV70025, TPS73325,TPS79325等等。
可是我一直矛盾于TPS72325的指标,他的输出电流就能达到200mA,会影响后续电路的使用么?
TPS72325事实上能够提供200mA以上的连续负载电流,只要您后续的电路最大电流不要超过200mA就没有问题。同时您需要注意一下散热设计,按照datasheet: www.ti.com.cn/.../tps72325.pdf 第二页参数。
所以您的顾虑是负载电流最大可能达到235mA, 而超过了TPS72325推荐的最大输出电流200mA. 而事实上TPS72325的输出电流保护点在300mA, 所以最大负载235mA时并没有问题。
建议您在TI网站上申请免费样片实际测试一下,输出电压是否符合需求(输出电压可能略微偏移),以及注意散热设计,避免芯片温度过高。
或者选用500mA规格的LDO :UCC284-ADJ/UCC384-ADJ.