1、In the case of light load, whether the output is normal and whether there is a protection mode for light load
2、According to the Datasheet, when the load current is less than half of the ripple current, it will enter DCM. At present, the limit maximum ripple current I calculated is 0.82A. If the output current is less than half of this value, it will become DCM
3、My current output vout is set to 7.3V. Does the inductor current become discontinuous at 6V or 35V input voltage? Is there any impact on stability or peak currents?