This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ4050: The RSOC shows a large jump after the product is reactivated from shutdown mode.

Part Number: BQ4050


Hello, TI engineers,
After a complete charge and discharge cycle with the BQ4050, the product enters shutdown mode and then, upon reactivation, the RSOC jumps significantly (SOC jumps from 25% to 65%). This is not an isolated issue but a widespread phenomenon. Is there any way to improve this problem?