This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS65217: 重复上电偶发无法启动

Part Number: TPS65217

TPS65217用作 AM335X 的电源。

连接5V 电压源为 TPS65217供电。 同时一个超级电容器储能经TPS61023DRLR稳压到4.2V后连接VBAT。

在断电一段时间内重新上电,偶发TPS65127无法正常重启。必须二次上电或长时间放置后重新上电,TPS65217才能正常重启;

上电不能重启时测量VBAT电源电压已经小于100mV。

另外,如果超级电容稳压后的电源接到USB,给AC和USB同时上电,会造成稳压芯片TPS61023DRLR短路击穿。

问题1:

   储能电容电路连接在VBAT上时,如何避免上电无法重启;

问题2:

   AC和USB端口是否可以同时供电?如果可以,需要注意什么事项?损坏外部稳压芯片TPS61023DRLR的可能原因是什么?

谢谢