Hi,
我在网上申请的程序用CCS6编译不出 .X0 文件,出现以下问题:
Invalid project path: Include path not found (C:\HSFBFirmware-1.0\HSFB\Pmbus).
Invalid project path: Include path not found (C:\HSFBFirmware-1.0\HSFB\UCD3138_Header Files).
This project contains unresolved buildable linked resources. It might not build as expected.
This project is currently in 'manual' Parser Preprocessing mode - no dependency graph is automatically generated. This mode should only be temporarily used to generate various pre-processor listing files. Please switch the Parser Preprocessing mode back to 'automatic' for you regular builds.
This project was created using a version of compiler that is not currently installed: 4.9.1 [ARM]. Another version of the compiler will be used during build: 15.9.0. Please go to <a href="liveaction:OpenAppCenter">CCS App Center</a> to install the compiler of the required version, or migrate the project to one of the available compiler versions by adjusting project properties.
将 Include 的错误修正后问题如下:
This project contains unresolved buildable linked resources. It might not build as expected.
This project is currently in 'manual' Parser Preprocessing mode - no dependency graph is automatically generated. This mode should only be temporarily used to generate various pre-processor listing files. Please switch the Parser Preprocessing mode back to 'automatic' for you regular builds.
This project was created using a version of compiler that is not currently installed: 4.9.1 [ARM]. Another version of the compiler will be used during build: 15.9.0. Please go to <a href="liveaction:OpenAppCenter">CCS App Center</a> to install the compiler of the required version, or migrate the project to one of the available compiler versions by adjusting project properties.
将 Complier Version 变到 15.9.0 问题如下:
This project contains unresolved buildable linked resources. It might not build as expected.
This project is currently in 'manual' Parser Preprocessing mode - no dependency graph is automatically generated. This mode should only be temporarily used to generate various pre-processor listing files. Please switch the Parser Preprocessing mode back to 'automatic' for you regular builds.