This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ25750: 充电电压异常,大于ACUV值5v才能正常充电,低于ACUV值时,适配器电压直接给电池充电

Prodigy 110 points
Part Number: BQ25750


TI工程师你好:

我们目前正在调试bq25750芯片电路,现在遇到一些关于ACUV相关问题,电路设置的ACUV是40v,电池电压为25v,充满是29v。

1、ACUV采用电阻硬件设置为40V,在适配器43v输入时电池充电电压只有8v,适配器电压调制45v,电池充电电压正常,这是什么原因导致的?和ACUV值必须保持5v压差吗?

2.当低于ACUV时,如39v时,电池充电电压39v,适配器电压直接给到了电池, ,而数据手册中提到,当VAC电压超过ACUV/ACOV 工作窗口,且SYS 电压低于 电池电压时,BATFET 才会导通。我们的电池电压为25v,与39v相比相差很大,为什么BATFET会导通,使39v直接施加到电池端。

3.当电路板未连接适配器,即VAC无电压时,将电池连接到电路板上,接下来再连接适配器45V,电路板指示灯不亮,电池被适配器直接充电。这个问题和2二个基本一致,就是由于VAC电压低于ACUV而导致适配器直接给电池充电。

以上是我们调试过程中遇到的问题,希望能得到你的解答