This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ24133“具有 EMI 合规性的集成 1-3S 独立电池充电器参考设计”中的MOS管开启问题

Other Parts Discussed in Thread: BQ24133

TI员工您好,最近在用BQ24133做电源管理,电路使用的是“

  • 具有 EMI 合规性的集成 1-3S 独立电池充电器参考设计

”中的电路。板子焊接后有以下问题:

1、充电电流不能过大,大于600maACFET会发热。

2、控制MOS管开关的电压ACDRV和BATDRV,输出电压不是芯片手册给出的典型电压。具体表现为:1插入适配器后,ACDRV只比CMSRC大1.3V,达不到MOS的开启电压。同时/BATDRV的电压和ACN相同(这个电压正常)。2去掉适配器后,ACDRV、CMSRC都为0V(不知道是否正常)。同时/BATDRV为2.2V、ACN位7.5V。(这个应该可以工作吧)。VREF3.3V,OVPSET1.06V

希望可以尽快解答。