This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ucd7242温度很高

Other Parts Discussed in Thread: UCD9222, UCD7242

用UCD9222和UCD7242套片给6678供电,方案、UCD9222固件同评估板。两路输出(1.0v和0.9v)正常,但0.9v输出通道温度偏高:

在6678时钟没有给的情况下,0.9v电流3A不到,但温度65度左右。当6678的时钟给出后(此时6678出于复位状态),

0.9v电流基本不变,但温度一直上升,在有风扇的情况可以达到107度左右,同时12V供电电流上升。在FUSION界面上没有任何报错和警告。

有没有人碰到这种问题?