BMS使用BQ76952进行电芯电压采样,AFE的VSS和DSP的GND工地后连接到BAT-上,BAT-上连接有FUSE,当BMS开机正常工作时突然断开FUSE,下图中的红色采样电阻均会失效,阻抗变大。
请问为何在BAT-断开后采样电阻会失效?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
需要注意的是,与其他引脚相比,VC0的电压容限较低。
当你说电阻器失效时,你是说它们烧坏了还是别的什么?另外,你介意分享一下你为什么在那里有FUSE吗?
我还注意到,你的VC0没有一个接地的输入电容器。请参阅
以及下方链接的Figure 2-5 使用外部BJT的平衡电路