This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ25703A: Charge Current not accurate, set 256mA but charge 1024mA.

Part Number: BQ25703A

I set the charge current by :

I2C_Write_Register(0x02, 0x00);
I2C_Write_Register(0x03, 0x01);

which set a 256mA current.

However, I monitor a 1024mA charge current.

Why?

Thanks for your help!

  • 您好,

    已经收到了您的案例,调查需要些时间,感谢您的耐心等待。

  • Some further measurement is performed.

    I set the charge current to be 256mA.

    Then I measure the charge current to the barrery is 256mA indeed. ( My battery is 13V now. )

    However, I find that the input current ( output current of my 12V adapter) is 1.5A.

    If I unplug the battery, let the bq25703a circuit to power my system, the input current will be 0.3A.

    which mean that charge a (13V) 256mA current will consume (12V) 1A input current.

    The following image is my PCB layout. Gate path is highlighted.

  • It looks to me a board or design issue. To quick find the cause, my suggestion is to order a BQ25703AEVM and check the EVM  performance. 

    Maybe you can try to add 150pF gate capacitor on the bottom FETs in the meanwhile.