This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ25750: 无法给电池充电

Part Number: BQ25750


电池为8S的磷酸铁锂电池组,我原理图参考的TI的评估板,硬件配置最大充电电流为2.5A、充电电压的设定电阻为14.7K,即充电电压27.6V,VFB采用默认的1.536V。测试时VAC(外部充电器)输出电压是28.4V,无法给电池充电。我用稳压电源测试时,设定输出电压为28.5V~28.6V时,充电电流最高为1A,无法超过2A。但是当我增加稳压电源输出电压到28.8V之后,充电电流能超过2A。想问下这是什么原因导致的?BQ25750_charger.pdf

  • 您好,

    已经收到了您的案例,调查需要些时间,感谢您的耐心等待。

  • 让我总结一下这些问题,以确保我理解正确。
    场景1: VAC=28.4外部充电器。No charging
    场景2:VAC=28.5V~28.6V。电池电流为1A。
    场景3:VAC=28.8V。电池电流可能超过2A。
    我有几个问题可以帮助调试:
    BQ25750充电时,您能测量SW1和SW2吗?
    你能把电感器的数据表发给我吗?
    在BQ25750充电时,您能把 register file发给我吗

  • 问题已解决。是我电路中VAC的工作窗口太小的原因。原先VAC(适配器)通过电阻器设置在25V~30V之间,导致VAC低于28.5V无法有效充电。现在我将VAC的工作窗口设定在23V~31V,当VAC在28V也可以正常充电。