This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Boost IC

Hi 

請推薦適合Boost IC 條件如下

        Power system request

Battery input 3.4V~4.2V 1200mAh

Output power A:

Amp 12V peak I=2.6A Avg:250mA

Output power B:

5V 100mA (HDMI audio codec Chip use)

PS: The 12V 5V system can be turned off when the system is shut down or in standby

Please provide an appropriate solution