This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LP8866S-Q1: LP8866S-Q1的调光问题

Part Number: LP8866S-Q1

LP8866S-Q1设置为混合模式(hybrid mode),将led设置为500ms延时渐变模式(SLOPE_SELECT位)。
I2C设置 
LED_CURR_CONFIG这个寄存器,将电流设置为1mA,将pwm占空比设置为10%,此时led灯位亮度1;
此时执行两条程序,先将电流设置为10mA,再将pwm占空比设置为1%,此时led灯位亮度2;
由亮度1到亮度2的过程,led会亮闪(或者说爆闪)一下再变成亮度2。

请问这种现象合理吗?如何解决led灯亮闪一下的问题呢。我们想让led亮度逐渐变化,避免爆闪或者亮闪一下的现象。谢谢!