This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ25756: BQ25756是否能实现100A的充电电流方案?

Part Number: BQ25756

rt,thx!

  • 已经收到了您的案例,调查需要些时间,感谢您的耐心等待。

  • 感谢您对TI产品的关注!
    关于你的咨询,BQ25756是一款多功能的集成电源管理IC,支持max高达20A的充电电流,具体取决于其配置和外部组件,如电感、电阻等。然而,要实现100A的充电电流,单纯依靠BQ25756可能不足,因为它的最大设计电流限制较低。

    如果你需要达到100A充电电流方案:
    可能需要并联多个BQ25756模块,以分担总电流。这需要确保每个模块的同步、均衡和安全设计。
    但暂时我们还没有类似的参考设计。