This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于UCD9222的相关疑问

Other Parts Discussed in Thread: UCD9222, UCD7242

目前设计一款6678的板子,发现电源这块比较容易出现问题。所以我现在设计一块小板子,上面仅仅是电源部分的。

在用UCD9222+UCD7242上,如果我在UCD9222上,不加入DSP的4个VID信号,UCD是否可以稳定输出1V呢?

因为那4个VID是监控DSP的,我想如果没有这4个信号的话,应该输出一个稳定值吧?