This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ25672: 请推荐一款适合太阳能光伏板充电的MPPT芯片方案

Part Number: BQ25672


你好,
我们公司在寻找一款太阳能充电的MPPT芯片方案,请推荐几款合适的芯片型号,给出spec和原理图参考设计等资料。
1,太阳能板开路电压6V,短路电流是12.9mA。具体参数见附件。
2,后级充电锂电池是4.2V截止充电电压
3,MPPT需同时给锂电池和后级负载供电(2A左右)。负载大概3V左右。即要求MPPT的带负载供电电压是降压且可调节电压,最好能和锂电池充电电压分开。
4,我们太阳能板6V,加载到锂电池上面充电,拉下到4.2V,这样直接充电效率比较低,所以我们引入MPPT,希望提升充电效率。
5,如果MPPT可以实现锂电池过压过流欠压欠流监测,则最好。

6,是否有开发板可测试?请给出验证其工作效率的方法建议。