I'm using TI's USB Interface Adapter and encountered an issue when modifying VADJ to 1.8V.
After powering on the ZC706, following the tutorial, the system prompted "Please Cycle Board POWER [off/on] and press OK when done" after running the XML for a while. Upon clicking OK, an error appeared:
"Failure occurred. READ_VOUT on rail #1 (0.001 V) was not within 5% of VOUT_COMMAND (1.000 V)"
According to the ZC706 datasheet, I noticed that Rail #1 of the UCD9012 is VCCINT.
What steps should I take next to resolve this error?
Here is the image.