This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ25672: 是通过芯片硬件本身即可实现MPPT吗

Part Number: BQ25672

你好,

1,这个BQ25672芯片,是硬件本身就可以实现MPPT功能吗,具体通过哪些PIN关联MPPT呢?

2,如果是需要通过外面MCU软件算法实现MPPT,那软件demo是否有链接可以参考?

3,手册写的是 低电池静态电流仅使用电池工作时为 17μA,充电器关断模式下为 500nA。相当于是电池倒灌给芯片的漏电流对吧?我们用于物联网,要求极低的漏电流,请问是否有500nA左右的MPPT芯片?