This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5148: 主MOSFET关断后出现短时驱动脉冲(非开关周期的下一个脉冲)

Part Number: LM5148


主要参数:

输入:22V~50V

输出电压:15V

输出电流:3A

开关频率:290KHz

问题1:

现象:输出电流2.5A以上输出电压下降,和限流现象相似,但不是限流(限流电阻12mΩ,限流阀值60mV,限制电流应该在5A左右),测试MOSFET和续流MOSFET驱动,在电流>2.5A时,关断后出现短时间脉冲,请问问题出在哪里了?

问题2:

计划测试开环测试进行问题排除,发现拆除功率电感后BUCK电源仍有输出电压,是什么原因?