This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ76925: The problem of shared sampling resistance between Gauge and Monitor

Part Number: BQ76925
Other Parts Discussed in Thread: BQ34110, BQ76952, BQ34Z100

As the question suggests, when I use BQ76925+BQ34110 to construct a BMS system, can the two chips share the same sampling resistor? I plan to connect the SRN and SRP of the two chips together, of course, I will use very short wiring to reduce adverse effects. I don't know if this is correct.

                                                                                                                                                                                                                                                                                                                                                 Sincerely!

                                                                                                                                                                                                                                                                                                                                                 Martain Bao.