您好,请问TPS62875-Q1的负载变化斜率可以支持到300A/us吗?如果负载以300A/us的电流变化斜率从轻载到重载变化时电源的电压跌落大概是多少?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,请问TPS62875-Q1的负载变化斜率可以支持到300A/us吗?如果负载以300A/us的电流变化斜率从轻载到重载变化时电源的电压跌落大概是多少?
您好,
可以使用堆叠方式。
请参考TPS6287x-Q1 2.7V to 6V Input, 15A, 20A, 25A, and 30A Automotive, Fast Transient, Synchronous Step-Down Converter With I2 C Interface datasheet (Rev. D) 中“10.3”和“10.4”中的电路应用。