Other Parts Discussed in Thread: BQ24166
BQ24166 系列
现象是输出电压只有2.7V左右,整个系统电压正常,可以正常上电,但是这款芯片工作时温升较大,在室温25℃下,工作30S,芯片表面温度就达到90℃了,整个系统的功耗在4W左右
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,
请参考Chipscale-Packaged bq24165/166/167 Evaluation Modules. (Rev. B)检查电路设计。
根据数据手册”THERMAL INFORMATION“,4W的功耗发热是正常的。
使用的是哪个封装的bq24166,QFN还是WCSP?
如果是QFN,芯片底部焊盘是焊接多少铜,是直接焊接在顶部,还是通过通孔连接到内部和/或底层?