最近用TPS62152做了一个4.1转3.3V的稳压电源,但是第一次测量的时候为3.1V,接上负载后变为了1,7V。后来重新焊接后,却变为了4.05V.怎么也稳不到3.3V。测量了一下PG引脚没有被拉高。是什么原因。电路和数据手册中的电路是一样的。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
最近用TPS62152做了一个4.1转3.3V的稳压电源,但是第一次测量的时候为3.1V,接上负载后变为了1,7V。后来重新焊接后,却变为了4.05V.怎么也稳不到3.3V。测量了一下PG引脚没有被拉高。是什么原因。电路和数据手册中的电路是一样的。
我把后面的电感去掉了,从芯片输出直接为4V,没有降压。PG接出来的电阻换的时候有时候是1.4V,同样的电阻,有的却是4V.都是去掉电感进行测量的。没有负载。
电感是构成buck降压结构最重要的元件,不能去掉。电感感值太小满足不了CCM稳态需求,太大输出电流能力下降。参考datasheet的电感计算公式,实际电感选择稍大于计算值即可。
掉电时测量vin到sw ,sw到地阻抗,看看内部mosfet是否被损坏。
输出电容是否为正常的22uf电容。
芯片底部的thermal pad是否良好焊接到接地的铜箔。