最近需要使用MOS做高侧开关,
1、使用PMOS(如CSD25402)可以,但是RDSon在5-10mOhm,NMOS的阻抗稍低,
2、但是NMOS用在高侧做开关时,需要驱动器,TI有没有专用的高侧NMOS驱动芯片 或者分立的器件方案?
注:只需要驱动NMOS的开关即可,不需要开关电源用的NMOS驱动芯片
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
最近需要使用MOS做高侧开关,
1、使用PMOS(如CSD25402)可以,但是RDSon在5-10mOhm,NMOS的阻抗稍低,
2、但是NMOS用在高侧做开关时,需要驱动器,TI有没有专用的高侧NMOS驱动芯片 或者分立的器件方案?
注:只需要驱动NMOS的开关即可,不需要开关电源用的NMOS驱动芯片
电路保护上,想用两个NMOS back-to-back(消除MOS体二极管的影响)连接方式,这样可以实现双向截止,我使用过PMOS,但是TI的PMOS做的最好(导通阻抗最小为5mOhm)也就是CSD25404,在电流为5A时,压降在50mV以上,我想使用NMOS将压降降到10mV左右
Hi
如果是电平做驱动,可以增加带chargepump的驱动芯片,http://www.ti.com/lsds/ti/power-management/half-bridge-driver-products.page