要设计一个高频大功率电流源(可以扫频),大概40MHz左右的使用频率,电流输出能力50~100mA左右,电压输出能力5V左右;我现在是先使用DDS输出扫频电压信号,然后使用OPA进行跨导放大变成恒流源,但是输出电压到500mV就上不去了,频率到1MHz左右也开始衰减了;我同时也仿真了使用高频运放来做跨导放大电流,但是运放输出电流一般比较小,电压也是500mV左右就上不去,频率特性还行;请问各位大神还有什么绝招吗?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
要设计一个高频大功率电流源(可以扫频),大概40MHz左右的使用频率,电流输出能力50~100mA左右,电压输出能力5V左右;我现在是先使用DDS输出扫频电压信号,然后使用OPA进行跨导放大变成恒流源,但是输出电压到500mV就上不去了,频率到1MHz左右也开始衰减了;我同时也仿真了使用高频运放来做跨导放大电流,但是运放输出电流一般比较小,电压也是500mV左右就上不去,频率特性还行;请问各位大神还有什么绝招吗?