This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
LM3478是不是改变外部器件就可以输出电压达到8v,4
LM3478调整外部boost器件就可以使3.3v输入转为8v,4A的输出
如果输入满足条件,同时外部其他电路没有问题,就可以调节反馈电阻来达到8.4V.
我的意思是输出电压达到8v,电流达到4A,主要是电流能不能达到
选择合适的器件,可以的,但是3.3V
但是3.3v是什么意思,是电流达不到吗?还是难度有点大