This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS92200: 输出电感值的选取问题

Part Number: TPS92200
Other Parts Discussed in Thread: TPS92201

我的设计参数如下:

VOUT为1.5V,VIN为12V,ILED为100ma,Kind我取值0.3,Fsw为1MHZ,芯片型号为TPS92200

依据手册8.2.3.2.1 Inductor Selection给出的公式算出电感值为73μH,这显然是不太合理的,于是我将VIN改为5V,别的取值不变的情况下计算得出电感值为17.5μH,我认为这个电感值还是太大,我有以下几个问题:

1.如果我想尽量降低电感值的选取,有什么办法,当然了,输出电流ILED的精度也要尽可能的高,

2.如果我选择的电感值太小,会造成输出的电流波动过大吗,除此之外,还会造成什么影响,

3.其他参数不变,我使用VIN5V和VIN12V两个参数时,芯片发热一样吗,如果不一样,差距会很大吗

4.除了TPS92200外,我还使用了TPS92201芯片,根据我的设计参数来选择,我发现手册推荐的电感值为2.2μ,但手册里并没有电感的计算公式,请问这里的电感值怎么计算得出呢,与TPS92200芯片手册里的计算公式一样吗,我按照该公式计算出来的电感值远远大于2.2μH