This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

求AC-DC 多负载方案



大家好,麻烦推荐一个 AC180-265V---DC12V 3A  & DC24V 2A 的方案,谢谢!

记得之前WEBENCH 还是有多负载方案的,不知道为什么今天只能选择单负载.

  • 亲;这个功率比较大。可能用WEBENCH会比较麻烦。好在变压器输出与匝数基本成正比,建议将24V2A等效并在12V上;成为12V7A输出。实际设计时;再翻开就好了。

  • 非常感谢。我就是被困在变压器这个环节,由于产品需要做认证,变压器规格我一直不知道怎么定,而WEBENCH又不提供型号,对于新手,好痛苦!

    还有,WEBENCH给的效率都在90%以上,可是实际很难做到。下图是我找的一个变压器规格,麻烦帮忙看看怎么样。