This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

dm648 ping不通



用的ndk-2.0.0 运行helloWorld程序后,提示:

TCP/IP Stack 'Hello World!' Application

Using MAC Address: 90-d7-eb-c5-cb-ba

cpsw_MDIO_Init

SetPhyMode:000021E1 Auto:1, FD10:64, HD10:32, FD100:256, HD100:128, FD1000:8192 LPBK:0

cpsw_MDIO_Init

SetPhyMode:000021E1 Auto:1, FD10:64, HD10:32, FD100:256, HD100:128, FD1000:8192 LPBK:0

EMAC should be up and running

EMAC has been started successfully

Registeration of the EMAC Successful

cpsw_MDIO_FindingState: PhyNum: 1

cpsw_MDIO_FindingState: Timed Out looking for a Phy!

cpsw_MDIO_PhYReset(1)

Enable Phy to negotiate external connection

NWAY Advertising: FullDuplex-1000 FullDuplex-100 HalfDuplex-100 FullDuplex-10 HalfDuplex-10

Network Added: If-1:192.168.1.43

Negotiated connection: FullDuplex 1000 Mbs

Link Status: 1000Mb/s Full Duplex on PHY 1

cpsw_MDIO_FindingState: Timed Out looking for a Phy!

cpsw_MDIO_FindingState: Timed Out looking for a Phy!

在PC端用PING 192.168.1.43 不通,但网络提示1G运行正常,不知怎么回事?