请问C6746的中断矢量表在哪一个说明文档中?看了几个文档,都没有关于这方面的说明。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Shine Zhang,谢谢你的回复,我想找到的是和C2000系列类似的,比如说INT1.4为XINT1,INT1.2为XINT2,这种具体的中断矢量表。因为我想设置两个外部中断,但是不知道它对应的矢量表。
中断事件在数据手册第88页上。
http://www.ti.com/lit/ds/symlink/tms320c6746.pdf
这些中断事件可以通过Interrupt controller映射到12个INT中断向量表。
Chapter 7
http://www.ti.com/lit/ug/sprufk5a/sprufk5a.pdf