关于6678工程建立问题有点疑问啊,我看论坛里讲的在多核程序编写时是通过DNUM来确定不同核,然后让不同核执行各自不同代码的。想问一下这里能不能够针对8个核建立8个工程分别生成8个out文件下载然后进行核间调试,如果可以该怎么弄???谢谢谢谢!!!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
可以在CCS中建立8个工程,分别编译生成8个out文件。
调试的时候建立debug session之后,分别把这8个out下载到对应的核中就可以了(下载的时候可以指定每个核下载的out文件).
但是一般如果多核工程代码都相同的话,建议一个工程,然后同时下载到8个核中运行会更加简单一点。
你可以看一下论坛置顶的帖子,里面有很多多核的例程。
一个最简单的多核工程,可以参考这个IPC的例子:
http://www.deyisupport.com/question_answer/dsp_arm/c6000_multicore/f/53/p/1056/2535.aspx#2535