This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DM6467+THS8200支持CVBS格式输出吗?

Other Parts Discussed in Thread: THS8200

看了下THS8200手册,支持YPbPr,RGB两种输出方式,不过没看到支持模拟CVBS输出?请问THS8200可以配置成一路或多路彩色CVBS(PAL或NTSC)输出吗?怎么配置?

  • 4.8.1 on datasheet  , it says:

    For component video applications, the nominal voltage level is 0.7 V; 1.305 V is used in NTSC/PAL composite video

    display. For composite video applications, the digital video stream must be encoded in an external digital NTSC/PAL

    encoder. The THS8200 only converts the digital composite signal to analog composite video.

    6.1

    Its ITU-R.BT656 output port could be used to connect to an NTSC/PAL video encoder, such as the Texas Instruments

    TVP6000, for regular composite/S-video output.

  • 0.7V is used for component,1.305 used for composite, if this means component and composite can not be usd at the same time even if external digital NTSC/PAL encoder is used?