大家好,
我这边板子做出来后,不焊接器件,测量C6670的CVDD引脚以及CVDD1引脚对地不短路。
焊接所有器件之后,测量C6670的CVDD引脚以及CVDD1引脚对地短路,万用表测量电阻<1Ohm。
想问下,正常的,C6678或者C6670,测量CVDD以及CVDD1(UCD7242一侧)对地电阻大概是多少???
谢谢!!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
谢谢Allen!!
我只焊接了一块板子,所以我自己没法横向做测试。
我再描述一下我的情况吧:
1. 我先是焊接所有器件,除了C6670,然后把UCD9222+UCD7242的电源调好。UCD9222一个通道的PWM同时控制两片UCD7242,输出CVDD,最大20A;UCD9222另一个通道的PWM同时控制另外两片UCD7242,输出VCC1V0,最大20A。如下图,
2. CVDD、VCC1V0输出正常后,我去补焊了C6670,然后上电,UCD9222报fast oc fault或者oc fault的错误。然后我再测C6670的CVDD以及CVDD1对地电阻小于1欧,才感觉是不是短路了,所以电流一下子就会过高,然后UCD9222报错?
谢谢Allen!!!
我又调试了一下,之前我是用Advantech的EVM6670的UCD9222配置,后来换成EVM6678的UCD9222配置。
目前情况是:CVDD1能正常输出1.0V,CVDD还是没法正常输出0.95V,UCD9222报错FLT。
所以我遇到一个非常奇怪的现象,就是之前UCD9222控制两片UCD7242输出CVDD1,我测得CVDD1对地电阻小于1Ohm,然后经过一些操作(换UCD9222配置、板子其他部分2、3个电阻替换),然后CVDD1电压输出就正常了,电压1.0V电流2A左右,CVDD1对地电阻11Ohm左右。
CVDD1之前对地电阻小于1Ohm,现在变成11Ohm了。。。。这很奇怪啊!!这期间做的改动主要是UCD9222控制CVDD1这路的软件配置,硬件上基本没动。
目前CVDD还是对地小于1欧,因为UCD9222控制UCD7242输出CVDD以及CVDD1的两路电路原理图完全一样,所以我把CVDD1那路的UCD9222配置拷贝到CVDD那一路,但是CVDD仍然无法输出正确电压,报错FLT。
请帮我再简单分析一下吧!非常感谢!
从DSP的角度看,你可以检查上电顺序是否正确,CVDD应该配置成默认电压1.1V。
其它的需要到Power的论坛咨询UCD9222的问题,我不太了解UCD9222的配置。