8168+DVRRDK
使用IOUTA~IOUTC,连接到视频放大器,再引出RGB信号,行、场信号用的AR8和AL9。
uboot启动时,没有输出logo。测量IOUTA~IOUTC,都没有波形,一直是0V。行、场信号也没有波形
参考
http://e2e.ti.com/support/dsp/davinci_digital_media_processors/f/716/p/247546/867752#867752
操作如下
mw.b 0x81000000 0xFF 0x300000
tftp 0x81000000 samplelogo_640x480.bmp
nand erase 0x00280000 0x300000
nand write 0x81000000 0x00280000 0x300000
setenv bootcmd ' logo on 0x280000 0x81000000 0xA0000000 40 60'
重启之后,uboot无法进入命令行
看到有人说修改device.c中的
omap_mux_init_signal("tsi5_bytstrt", OMAP_MUX_MODE2);
omap_mux_init_signal("tsi5_pacval", OMAP_MUX_MODE2);
可是这个c文件是在kernel中的,并不在uboot中,应该不是这个问题。
问题一:RDK是否支持从模拟DAC接口输出boot logo
问题二:如何确认uboot是否对DAC进行了配置
在cmd_logo_816x.c中看到了如下语句
/*enable the DAC_CORE*/
WR_MEM_32(0x48140660, 0x1);
/*set the HSYNC/VSYNC for HDCOMP, use DVO1 signal, this
is for PG2.0 or above silicon only*/
if ( get_cpu_rev() >= PG2_0) {
/*these settings matches DVR reference,
it may not work with DM816X EVM*/
WR_MEM_32(0x4814086c, 0x2);
WR_MEM_32(0x48140870, 0x2);
WR_MEM_32(0x48140724, 0x2);
可是用md命令读0x4814086c和0x48140870,返回全是0。
https://e2e.ti.com/support/dsp/davinci_digital_media_processors/f/717/t/240982
里边提到可以查看寄存器设置,请问查询命令是什么。试过mdump,提示非法命令。
问题三:管脚复用问题
手册P262中
For example, these are the steps required to use the pins AR8 and AL9 as the DAC_HSYNC and VSYNC signals:
1. Set the PINCTRLx registers for AR8 and AL9 as follows:
• 0x4814 0894 = 0x00000001
• 0x4814 0898 = 0x00000001
2. Select analog VENC sync out option as follows:
• 0x4814 0724 = 0x00000004
cmd_logo_816x.c中的
REG32(CSL_TI816x_CTRL_MODULE_BASE + 0x0894) = 1; //37 tsi7_bytstrt vout0_fld
REG32(CSL_TI816x_CTRL_MODULE_BASE + 0x0898) = 1; //38 tsi7_pacval vout0_avid
/*enable the DAC_CORE*/
WR_MEM_32(0x48140660, 0x1);
/*set the HSYNC/VSYNC for HDCOMP, use DVO1 signal, this
is for PG2.0 or above silicon only*/
if ( get_cpu_rev() >= PG2_0) {
/*these settings matches DVR reference,
it may not work with DM816X EVM*/
WR_MEM_32(0x4814086c, 0x2);
WR_MEM_32(0x48140870, 0x2);
WR_MEM_32(0x48140724, 0x2);
是否需要将WR_MEM_32(0x48140724, 0x2);改为WR_MEM_32(0x48140724, 0x4);
问题四:uboot启动时,会在串口输出如下字符图形,该图形是否可以修改?
:,;;:;:;;;;;;;;r;;:,;;:;:;;;;;;;;:,;;:;:;;;;;;;;:,;;:;:;;;;;;;;:;;;;;;;;:,;;:;:
;,;:::;;;;r;;;rssiSiS552X5252525259GX2X9hX9X9XX2325S55252i5:,;;:;:;;;;;;;;:,;;:
;:;;;;;;;rrssSsS52S22h52299GGAAMHMM#BBH#B#HMM#HMBA&&XX2255S2S5Si:,;;:;:;;;;;;;;
;:;;r;;rsrrriiXS5S329&A&MH#BMB#A&9XXA252GXiSXX39AAMMMBB&G22S5i2SSiiiisi:,;;:;:;
;;;;;r;rr2iisiih393HB#B#AA99i22irrrX3X52AGsisss2Xii2299HBMA&X2S5S5iSiisSsi:,;;:
r:r;rrsrsihXSi2&##MHB&Ahh3AGHGA9G9h&#H##@@@##MAMMXXX9SSS29&&HGGX2i5iisiiisisi:,
;;rrrrsSiiiA&ABH&A9GAGhAhBAMHA9HM@@@@@@@@@@@@@@@@@@@HHhAh2S2SX9&Gh22SSiisiiisii
r:rrssisiS2XM##&h3AGAX&3GG3Ssr5H@M#HM2; ;2X&&&MHMB###GBB#B&XXSSs529XX55iSsisisi
r;rsrisSi2XHAhX99A3XXG&&XS;:,rH#HGhAS @@@@3rs2XBM@@A552&&AHA2XiisSS252SSsisSs
r;issi5S22&&3iSSX292&hXsr;;:;h@&G339&S9@@@@2@MA&9&HB##Xris29ABMAAX2ir;rsSi5iss5
rrsSi2XhG&9GXh399&X99i;;;;;;r#H&293H9X#@@@@@@@B&9GhAH@XrrsrsiXABHB&HG2rr;rrSiSi
;:rsisS599&AA9XG&3A35r;:::;,;BMh&&2iX5A@@@@@@@&392X5GB2;;;r;iSX393A##A&Xi:::rsi
;:rss552222X553&XHMhir;;::,:,h#HhGSXhG3#@@@@#AXXS2XAHA;::;;;;ss55XShBA3239r:,;;
r;ii2S5SSi2i53hirsh2srr::,,,,;MMXX359&Ah3h&Si59SX99A#i:,::::;;sri2,.2r;:SGAr;,:
;:;rrrrssiriXGSi::shs;;;,,,:,,rBBA9h5s5h5iS5isi2SAHB5:,,,:::;rrs5&SrisSX5Srrr:,
;,r;;;;rsriSSrrrr;;5Xrr;;,:,,.,;9AA2SsisS5323XXXG9&i:.,,::;;r;;;srrrrrr;;:;::::
:,;r;r;rrissrrr;:;::;s;;;;,:,,..,r293h222hXXAAGGGX;:,,,:,:,::;:;::,:,,,,...,,,,
;,;;;;rrrrrrrrirr;,.,,:::::::,,,,.,;SX&ABAB2hhXir:,,.,,.,,:,,,,..,,,..,..,,,..:
:.:;:;;;:;;;;r;rrs;:.. ,,:::::,:,:,,.::rrsrr;;,,.......,..,....,,,,,,,...,.,,:,
:.:::,::::::;;r;rrr;:.......,.,.,,:::,,...............,,::.,,,,:,::,,:,:,,,:,;:
,.::,:,,,,,;;;;;;;;r;;::,..............................;;;:;::::,:::::::,:,:,,,
: ,,:,,,,,,,,,,,,,:;rrr;;:;,,,,,,,::,.,.:.,.,;s,:;;;;:;:;;;;;::::,:::,:::,:,:,:
,.,,,,,,,...,,.,,....................................:,............:,,,:,:,,,,,