This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

IBL编译问题,在运行脚本时,sed -e expression #1 ,char 8 untermination 's' command

1 sed -e expression #1 ,char 8 untermination 's' command 不知道如何修改

2 同时最后的编译结果是:mv:cannot stat  '../../../i2crom_0x51_c6678_le.bin' :No such file or directory

                                               mv:cannot stat  '../../../i2crom_0x51_c6678_be.bin' :No such file or directory

mv:cannot stat  '../../../i2crom_0x51_c6670_le.bin' :No such file or directory

mv:cannot stat  '../../../i2crom_0x51_c6670_be.bin' :No such file or directory

mv:cannot stat  '../../../i2crom_0x51_c6657_le.bin' :No such file or directory

mv:cannot stat  '../../../i2crom_0x51_c6657_be.bin' :No such file or directory

mv:cannot stat  '../../../i2crom_0x51_c6657_le_0x500.out' :No such file or directory

mv:cannot stat  '../../../i2crom_0x51_c6657_be_0x500.out' :No such file or directory

 有6678和6670的out文件

我现在想在ibl内去配置ibl的参数,重新编译

void main (void)
{
    int32 i, j;
    UINT32 v, boot_mode_idx, boot_para_idx;
    unsigned int dip_setting;
    ibl_t ibl;
  
    /* Initialize the status structure */
    iblMemset (&iblStatus, 0, sizeof(iblStatus_t));
    iblStatus.iblMagic   = ibl_MAGIC_VALUE;
    iblStatus.iblVersion = ibl_VERSION;

    ibl = c6657_ibl_config();
   
    /* Init UART */
    uart_init();
    uart_write_string("", 0);
    uart_write_string("IBL version: "ibl_VERSION_STR, 0);

。。。。

在主函数内加了ibl = c6657_ibl_config();

其他的参数修改在device.c内

我修改的脚本文件

1 tools_build.bat

    set path=C:\MinGW\msys\1.0\bin;C:\MinGW\bin
    C:\MinGW\msys\1.0\bin\bash IBL_buildibl

2 setupenvMsys.sh

#!/bin/bash

# Environment setup to be done if using MSYS Bash shell for build

# Specify the base directory of the c6000 compiler with UNIX style path separator
#export C6X_BASE_DIR='"C:/Program Files/Texas Instruments/C6000 Code Generation Tools 7.2.4"'
export C6X_BASE_DIR='"C:/ti/C6000 Code Generation Tools 7.4.0"'

# Specify the base directory of the c6000 compiler in format understandable by the MSYS Bash shell
#export C6X_BASE_DIR_MSYS=/c/Program\ Files/Texas\ Instruments/C6000\ Code\ Generation\ Tools\ 7\.2\.4
export C6X_BASE_DIR_MSYS=/c/ti/C6000\ Code\ Generation\ Tools\ 7\.4\.0
# Don't modify the below variables. They are derived from the above definitions


export PATH=$PATH:$C6X_BASE_DIR_MSYS/bin
export TOOLSC6X=$C6X_BASE_DIR
export TOOLSC6XDOS=$C6X_BASE_DIR