Part Number: PROCESSOR-SDK-AM62X
In ti-processor-sdk-linux-rt-am62xx-evm-10.01.10.04,I want to use the CJC8990 as the audio codec on the AM62X chip, but the following error occurred when I was using it.
:~#aplay -l
**** List of PLAYBACK Hardware Devices ****
card 0: cjc8990hifi [cjc8990-hifi],device 0: 2b10000.audio-controller-cjc8990-hifi cjc8990-hifi-0 [2b10000.audio-controller-cjc8990-hifi cjc8990-hifi-0]
Subdevices: 1/1
Subdevice #0: subdevice #0
:~##speaker-test -c 2 -t wav
speaker-test 1.2.11
Playback device is default
Stream parameters are 48000Hz, S16_LE, 2 channels WAV file(s)
Rate set to 48000Hz (requested 48000Hz)
Buffer size range from 16 to 131072
Period size range from 8 to 16384
Periods = 4
was set period_size = 12000
was set bufer_size = 48000
0 - Front Left
Write error: -5,Input/output error
xrun_recovery failed: -5,Input/output error
Transfer failed:Input/output error
My dts configuration is as follows:
main_macsp1_pins_default: main-mcasp1-default-pins {
pinctrl-single,pins = <
AM62X_IOPAD(0x0124, PIN_OUTPUT, 1)
AM62X_IOPAD(0x0128, PIN_OUTPUT, 1)
AM62X_IOPAD(0x0114, PIN_OUTPUT, 1)
AM62X_IOPAD(0x010c, PIN_INPUT, 1)
>;
};
cjc8990_mclk: clk-0 {
#clock-cells = <0>;
compatible = "fixed-clock";
clock-frequency = <12288000>;
};
codec-audio: sound {
compatible = "simple-audio-card";
simple-audio-card,name = "cjc8990-hifi";
simple-audio-card,widgets =
"Headphone", "Headphone Jack",
"Line", "Line In",
"Microphone", "Microphone Jack";
simple-audio-card,routing =
"Headphone Jack", "LOUT1",
"Headphone Jack", "ROUT1",
"LINPUT1", "Line In",
"LINPUT2", "Line In",
"Microphone Jack", "Mic Bias";
simple-audio-card,format = "i2s";
simple-audio-card,bitclock-master = <&sound_master>;
simple-audio-card,frame-master = <&sound_master>;
simple-audio-card,bitclock-inversion;
simple-audio-card,cpu {
sound-dai = <&mcasp1>;
};
sound_master: simple-audio-card,codec {
sound-dai = <&cjc8990>;
clocks = <&cjc8990_mclk>;
};
};
&main_i2c0 {
status = "okay";
clock-frequency = <100000>;
rtc0: rtc-pcf8563@51 {
compatible = "nxp,pcf8563";
reg = <0x51>;
#clock-cells = <0>;
};
cjc8990: audio-codec@1b {
#sound-dai-cells = <0>;
compatible = "cjc8990";
reg = <0x1b>;
clocks = <&cjc8990_mclk>;
clock-names = "mclk";
ai3x-micbias-vg = <1>;
AVDD-supply = <&vcc_3v3_sys>;
IOVDD-supply = <&vcc_3v3_sys>;
DRVDD-supply = <&vcc_3v3_sys>;
};
};
&mcasp1 {
status = "okay";
#sound-dai-cells = <0>;
pinctrl-names = "default";
pinctrl-0 = <&main_mcasp1_pns_default>;
op-mode = <0>;
tdm-slots = <2>;
serial-dir = <
1 0 2 0
0 0 0 0
0 0 0 0
0 0 0 0
>;
tx-num-evt = <0>;
rx-num-evt = <0>;
};
Please tell me how I should deal with this problem so that I can use the cjc8990 codec chip normally.
This is the schematic diagram,whether there is