This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM335x+AR8031网口ping不通



参考TI AM335x SSK开发板先做了一版实验板,做了四块(机器贴的)四块网口都能用,后来做核心板,原理图和开发板和实验板是一样的,手焊了两块核心板网口都ping不通,

打印信息如下:

U-Boot# ping 192.168.1.100
link up on port 0, speed 1000, full duplex
Using cpsw device
ping failed; host 192.168.1.100 is not alive
U-Boot# 

原理图是RGMII 千兆模式,原理图见附件

测试发现AM335X_RGMII1_TXCLK这个引脚启动时是10MHz,ping一下然后就变成50MHz 了,这个是不正常的,

实验板这个引脚启动时是25MHz,ping一下就变成125MHz,这是对的,

用的uboot代码是一模一样的。

现在就是不知道这个问题是那引起的?


AM335x+AR8031.pdf