C6746Z中断文档中说:The nonmaskable(NMI) is not supported on all C6000 devices.关于Nested interrupt 中又提到:However,when the interrupt service routine is for one of the maskable interrupts(INT4-INT15),An NMI interrupt processing of the maskable interrupt.不矛盾吗?
请问下,现在中断矢量表映射:定时中断-INT4,外部中断-INT5,可以使用外部中断-INT5来打断正在执行中的定时中断-INT4吗?