在DSPC674X上有这么一段:DMA writes code to L2 SRAM that is then executed by the CPU (this case is supported by the hardware protocol on C621x/C671x and C64x DSPs, but is not supported on C674x DSPs). (1)在以往的C64X平台, 我们是用DMA利用PING-PONG操作将数据读入L2RAM,然后CPU处理来节省数据读入Cache的时间,但是现在C674X平台不支持DMA拷入L2RAM,然后CPU再处理,该如何处理可以使用DMA传递数据然后CPU操作来像在C64X平台那样操作来达到从而节省数据读入Cache的时间呢? (2)现在在L2 RAM 和 DDR 上都做1920*1080次加法, 耗时是基本相同, 都是40ms, 这个是什么原因?