DM6467T的ATA接口与HPI接口可以同时使用吗?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
ATA能和HPI16bit同时使用, 不能和HPI32同时使用
第114页上的表Table 4-24. PCIEN, HPIEN, and ATAEN Encoding
我们主要有以下问题:
1、 DM6467的ATA、EMIF、HPI部分管脚复用,如果HPI使用16位模式,那么其只占用复用的低16位,ATA占用高16位,可以同时工作。但是如果需要FLASH存程序,那么EMIF接口需要使用,这样NAND FLASH、ATA、HPI同时使用,那么这个复用有没有解决的方法
2、 DM6467提供了一个VLYNQ接口,专门用来与FPGA通信,如果HPI、ATA、NAND FLASH实在不能同时共存,那么HPI如果改成VLYNQ接口连接,能否能够实现高带宽的数据流通道(VLYNQ接口数据率能达到多少)?