This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DSP5509 EMIF地址总线



1、看文档里面说,5509内部地址线24bit。按照数据存储空间使用时,地址编码采用字寻址方式,使用A1~A23共计23条地址总线访问存储器,此时A0无效。但时,数据传输过程中使用24条地址总线A0~A23,此时A0始终为0。

2、EMIF中对16bit的存储器写8bit的数据时,内部地址bit0表示MSB和LSB。

问题

一、5509接TL16C752用作串口时,地址线接的DSP上A1-A3,是不是就是第1条里面说的A0始终为0的原因?

二、第2条里面bit0跟第一条里面的A0是什么关系?